510-933-6200         Sales & Support         Locations         Login

              
Contact Us
Swagelok Northern California
Menu
BUY NOW
Message Us
Digital montage (1)

Fluid Systems Engineering & Management Blog

by Swagelok Northern California

As the Saying Goes, Don’t Judge a Swagelok Hose By Its Cover

by Jeff Hopkins, on 5/28/15 11:00 AM

Understanding how a hose is built from the inside out can make it easier to choose the right hose for your application


Swagelok Hose Solutions Poster SM
Get the Swagelok Hose Catalog, Quick Look, and Hose Solutions Poster Here »  

There's a lot more to a hose than what you can see from the outside. For instance, when we talk about types of hose, we're talking about the core of the hose. You may see a braided steel cover on a particular hose, but if the core is PTFE, then it's a PTFE hose.

Different core materials give the hose different qualities. Here are the basic types of Swagelok hoses you can order from Swagelok Northern California, and the qualities associated with each.

Metal hose

Metal hose is the best option for applications that produce very high or very low temperatures, up to 454C and down to -200C. They also handle pressures from 3100 psi to vacuum. On top of that, they aren't gas permeable. That's important if, say, you need to connect a bottle of gas to an analyzer and you don't want the gas to bleed off. Our FM and FL metal hoses exhibit strong performance in dynamic cycling applications, and our metal hoses with a 316L braid provide greater corrosion resistance.

Metal hose isn't perfect for everything, however. It's not recommended for high vibration applications, because vibration can cause fatigue failure. They also shouldn't be subject to pressure surges or shock where the pressure is greater than 50 percent of working pressure.

PTFE hose

PTFE hose offers great flexibility, and can handle pressures up to 3500 psi. We also can supply this hose with a variety of end connections, because we make them right here in Fremont. PTFE is a great choice because it is compatible with almost all media. There is only a short list of materials that do not work well with PTFE. If there's any concern about static electricity generation, we can supply a static dissipative carbon-filled PTFE core.

Hydraulic

Traditional hydraulic hose has a metal braid inside for reinforcement. It's strong, but the wires can break and puncture the core. That also makes the hose swell. Instead of wire, we use an internal fiber braid reinforcement to enhance the hose’s pressure rating. Our thermoplastic hydraulic hose has a smooth bore nylon core that can handle pressure up to 5000 psig, and it is available as a SAE general-purpose or SAE nonconductive nylon core. We also put on a polyurethane cover to resist abrasion, and the cover is perforated to prevent blistering.

Rubber

Rubber hose is a nice choice for low-pressure applications, up to 350 psi. You push on the end connection up to the shoulder of the fitting, and it's ready to go. A nice benefit is that the internal fiber reinforcement enhances the hose’s pressure rating and ensures connection retention. We offer it with a Buna N core in sizes from a quarter-inch to a full inch.

Special tagging for hoses

We also can tag your hose with a lot of information such as the date of purchase, purchase order number, part number and more.

Now when you tackle Swagelok's 88-page hose catalog, you'll be able to navigate with a bit more skill. To make it easier, we have created a hose quick look and hose solutions poster to help you find the hose you need faster.

Download the hose catalog, quick look, and poster here »

 

Additional Resources

Swagelok Hose Selection  Swagelok Hose Selection Tutorial  
Hose Selection Tutorials Hose Assembly Services  

Topics:Hoses

We perform under pressure

Your fluid systems can't fail—and they can't leak. That's why Swagelok Northern California offers mission critical solutions for the petrochem, semi, power, and oil and gas industries around the Bay Area and into NW Nevada. We manufacture and assemble reliable, customizable components that get the job done. Contact our team today to learn about custom solutions for your plant or refinery.