510-933-6200         Sales & Support         Locations         Login

              
Contact Us
Swagelok Northern California
Menu
BUY NOW
Message Us
Digital montage (1)

Fluid Systems Engineering & Management Blog

by Swagelok Northern California

Swagelok Pressure Gauge Selection and Installation Tips

by Jeff Hopkins, on 12/5/13 12:00 PM

Choosing and installing a pressure gauge is not always as easy as it seems


Swagelok-Pressure-Gauges-Catalog
Get access to Industrial and Process Swagelok Pressure Gauge catalogs here »

Choosing and installing a pressure gauge is not always as easy as it seems, so here are a few tips that should help simplify selection, ensure proper operation, and extend the service life of your gauges. 

Pressure range

In general, when choosing a pressure gauge, it's best to choose a pressure range that is roughly two times greater than the average pressure of your system. This gives sufficient over pressure protection and better accuracy.

For applications with constant, steady pressure, the measured pressure should be no more than 75% of the full scale range of the gauge. For applications with fluctuating pressure, the measured pressure should be no more than two-thirds of the full scale range of the gauge.

Sweet spot                   

A pressure gauge is usually most accurate in the middle third of the dial. When selecting a gauge, be sure that your normal system pressure falls within that “sweet spot”. For example, if your system pressure is 100 psi, consider using a 200 psi gauge.

swagelok pressure gauges

Some pressure gauge models are available with dial faces of different diameters. Normally the larger the dial diameter, the more accurate the gauge.

Proper orientation

To make a gauge easy to read it needs to be installed in the proper orientation so the dial face is pointing toward the user. Many gauge designs utilize pipe fittings to connect the gauge into a system and these pipe threads can make orientation of the dial very difficult.

To get the gauge dial to face the desired direction, often times the installer will either overtighten the gauge possibly damaging the pipe threads, or under-tighten the threads and possibly cause a leak.

swagelok pressure gauges

Swagelok Tube Adapters

Swagelok Pressure gauges offer a unique end connection option that simplifies installation when they are used with a Swagelok tube fitting.

Swagelok Pressure Gauge Swagelok Tube Adapter Tee resized 600

Gauges with integral Swagelok tube adapters eliminate alignment problems because the gauge dial can be aligned to the desired position and it remains stationary during pull-up of the fitting.

Swagelok Pressure Gauges

For more details on Swagelok Pressure Gauges available from Swagelok Northern California, check out our Industrial and Process Swagelok Pressure Gauge catalogs page »

 

Additional resources

Swagelok-Pressure-Regulators Selecting & Sizing Pressure Reducing Regulators
Swagelok Pressure Regulators Catalogs   Selection & Sizing of Pressure Reducing Regulators (13 pages)
Topics:pressure gaugesTraining

We perform under pressure

Your fluid systems can't fail—and they can't leak. That's why Swagelok Northern California offers mission critical solutions for the petrochem, semi, power, and oil and gas industries around the Bay Area and into NW Nevada. We manufacture and assemble reliable, customizable components that get the job done. Contact our team today to learn about custom solutions for your plant or refinery.