---
title: Ten Sampling System Mistakes Harming Your Operations
description: Protect your operation by avoiding these ten sampling system mistakes. Download the white paper, Ten Sampling System Mistakes Harming Your Operations today.
---

[Fluid Systems Engineering & Management Blog | Swagelok NorCal ](https://northerncal.swagelok.com/blog)

# [Ten Sampling System Mistakes Harming Your Operations](https://northerncal.swagelok.com/blog/ten-sampling-system-mistakes-harming-your-operations)

 Written by [Jeff Hopkins](https://northerncal.swagelok.com/blog/author/jeff-hopkins) | 2/16/17 4:30 PM

In this blog, get a summary of the Swagelok white paper, Ten Sampling System Mistakes Harming Your Operations, then download the four page white paper to get the complete picture,  [here »](https://northerncal.swagelok.com/important-sampling-system-mistakes-to-avoid/)

 

## Protect your operation by avoiding these sampling system mistakes

 

There are plenty enough challenges to managing an analytical instrumentation operation without unexpected downtime and maintenance costs. It takes a good sampling system design and good operations practices to keep the system performing well.

Check out these 10 mistakes that often are made with sampling systems. Avoid these, and you'll prevent a lot of headaches.

**1. Check for simple errors.**

Some mistakes are easy to spot, but can wreak havoc if you don't bother to look. They include reversed check valves blocking the sample flow, or a fast loop flowing backwards.

**2. Too much volume upstream of the first regulator**

High-pressure gas can cause condensation in the lines and actually slow things down because of gas compressibility. It can also be a safety concern if a component ever fails and causes rapid decompression.

**3. Low liquid sampling pressure**

Liquid samples are just the opposite. Too little pressure may release a dissolved gas, causing the liquid to bubble or foam.

**4. Paying too little attention to surfaces**

When sample fluid touches a surface, a few molecules stick. Loss of molecules due to absorption can spoil your sample. Pick the proper materials for filter elements, regulator diaphragms, tube walls, or gas cylinders.

**5. Elastomer seals not compatible with sample fluids**

Material that is mismatched to your sample fluid may cause a leak or even or even a blockage within the sampling device.

**6. Sampling from a stagnant line**

Samples always should come from an active process line, and should come from a point that gets the sample to the analyzer quickly.

**7. Dead legs in the sample-transport line**

Dead legs or unpurged volume allow molecules to diffuse into the sample causing a slow analyzer response and continuous contamination of the system.

**8. The vaporizer is too hot**

A hot vaporizer body could boil the incoming sample, causing it to fractionate.

**9. The sample flow is too slow**

The slower your sample flow, the more viscous drag is placed on the interior wall of your tubing, causing solids to form.

**10. Not looking for the causes of time delay**

If the measurement does not follow your process, you have time delay in your system. Other symptoms are blurred or muted response, laboratory disagreement, and poor performance of a control scheme. View a sample time delay calculation.

You can lean more details about these mistakes by [clicking here](https://northerncal.swagelok.com/important-sampling-system-mistakes-to-avoid) to download a white paper, complete with links to examples and formulas.

### [Download the four page white paper to get the full story](https://northerncal.swagelok.com/important-sampling-system-mistakes-to-avoid)

 

## Additional Resources

 

 

 

[View full post](https://northerncal.swagelok.com/blog/ten-sampling-system-mistakes-harming-your-operations)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Jeff Hopkins"
  },
  "dateModified" : "2017-02-16T16:45:30.734Z",
  "datePublished" : "2017-02-16T16:30:00Z",
  "headline" : "Ten Sampling System Mistakes Harming Your Operations",
  "image" : {
    "@type" : "ImageObject",
    "height" : 541,
    "url" : "http://northerncal.swagelok.com/hubfs/2016_COVERS/Ten-Sampling-System-Mistakes.png",
    "width" : 474
  },
  "mainEntityOfPage" : "https://northerncal.swagelok.com/blog/ten-sampling-system-mistakes-harming-your-operations",