Fluid Systems Engineering & Management Blog | Swagelok NorCal

Addressing Common Seal Support System Issues Proactively

Written by Paul Lesnau | 7/28/20 3:45 PM

No matter which Northern California petrochem refinery you work in—Concord, Martinez, or Benicia—the scene is common. You get the maintenance ticket for a horizontal pump that you’ve never done planned maintenance on before. It’s leaking. The pump hasn’t been shut down, but when you get there it becomes clear that mechanical seal failure is the root cause of the problem. 

You check the maintenance log and find that the seal was installed less than a year ago. Per the API, mechanical seals should last an average of three years. A quick review of the immediate pump environment reveals no obvious issues. What’s the problem? 

I’m here to help you sort it out. 

Seal Support System Issues That Lead To Failure

You’re probably familiar with the truism that mechanical seals fail when the seal support system no longer provides the required seal chamber environment to ensure reliable operations. To be a bit more specific, two major seal support system issues—temperature and particulates—inevitably lead to mechanical seal failure.

Let’s look at each of these with an eye toward proactively addressing the problems to prevent failure.

Temperature Takes a Toll

Changes in process fluid temperatures and/ or a seal support system’s inability to efficiently control seal chamber temperature can slowly, or in some cases, quickly lead to leakage. In older Bay Area refineries, seal support systems installed years ago, intended for certain process conditions, now contend with higher process fluid temperatures. As a result of elevated temperatures, there are a variety of effects: 

  • Elastomeric components such as o-rings degrade
  • Seal face dimensions change and ruin seal integrity
  • Plated seal faces crack, causing rapid wear of the carbon face
  • Corrosion increases, creating particulates that damage seal integrity

The inability of a seal support system to maintain the proper temperature in the seal chamber can be the result of numerous factors. The table below summarizes the issues and offers practical solutions to address them.

Seal Support System Issue 

Solution 

Inadequate cooling capacity 

  • Replace coils in existing cooler
  • Install larger capacity cooler
  • Replace cooler with heat exchanger
  • Upgrade to a serviceable cooling reservoir

Insufficient fluid circulation 

  • Add pumping ring to seal chamber to improve circulation and cooling
  • Increase the diameter of seal support system tubing for greater throughput of process fluid, barrier fluid, or flush fluid
  • Increase seal pot volume to supply buffer fluid to allow 
  • Add variable flowmeter to optimize circulation 

Seal chamber pressure increased by steam flush

  • Install pressure gauge to regulate steam and reduce pressure/ friction on the atmospheric seal face

Unexpected shutoff of barrier/ buffer fluid

  • Upgrade pressure and/ or flowmeter instruments with transmitters to provide immediate notification of interruption

 

Worth considering: Although not directly a part of a seal support system, the addition of a thermal bushing or heat slinger in the seal box can significantly limit high-temperature process fluids from migrating into the seal chamber and reducing mechanical seal life.


Particulates Provoke Problems 

As mentioned above, an increase in fluid temperature eventually correlates with increased corrosion throughout pipes and pumps, posing the potential to damage mechanical seal reliability. An increase in process fluid particulates, whether by corrosion or inherent in the process fluids, can lead to:

  • Build-up on the pump shaft that prevents free movement of the O-ring
  • Build-up on springs, bellows, and drive-rings that diminishes mechanical seal reliability

  • Deposits on portions of the seal faces causing a gap, with leakage increasing as the seal face degrades

Effective remedies for particulates include: 

⇒ Upgrading to inline, serviceable (in situ or once removed) T-type, F, FW, or TF filters with appropriate pore sizes

⇒ Adding a bypass line to facilitate planned filter cleaning or replacement without stopping the system flow

⇒ Upgrading to a cyclone separator to remove particulates without the need to clean or change a filter

Protecting pumps from the plague of corrosion via better filtering may be one of the easiest means of improving pump reliability.

Factors To Consider When Upgrading or Replacing Seal Support Systems

Proactive identification and remedying of these seal support system issues are the most cost-effective means to reduce unplanned downtime caused by pump leakage. But it’s not always a simple matter of “ordering from the catalog.” Upgrades and replacements should be undertaken with a holistic approach. 

Consider some of the many factors involved in selecting the right seal support system configuration for petrochem processing: 

  • Process fluid temperature 
  • Particulate size
  • Viscosity suction
  • Buffer/ barrier fluid selection
  • Discharge pressures 
  • Existing infrastructure
  • Pump Best Efficiency Point (BEP) 
  • Cal/OSHA and BAAQMD regulations

Guidance from experts who have “been there, done that” can simplify the complexity of upgrading or replacing inadequate seal support systems.

Take Advantage Of Local Seal Support System Expertise

At Swagelok, I’ve worked with rotating equipment engineers across Northern California refineries to find the right seal support solutions to meet their process needs. Our experienced Field Engineers consult with you at the plant to review the challenges in context of the specific pumping operations. You’ll get recommendations including detailed technical specifications, based on API 682 plans and configuration options to address these common seal support system issues.  

Upon your review and approval of Swagelok recommendations, we’ll then select the components, fabricate and test your seal support systems following the ISO 9001 process quality standards prior to delivery. Being local, with facilities in Fremont and Concord, we’re always available for technical support by phone or onsite. 

To find out more about how Swagelok Northern California can help address common seal support system issues by providing expert consultation and Assembly Services, Contact our team today by calling 510-933-6200.

About Paul Lesnau | Sales Manager, Business Development Manager, and Field Engineer

Paul holds a B.S. in Mechanical Engineering from North Dakota State University. Before joining Swagelok Northern California, he was the West Coast Regional Sales Manager for an organization based in Illinois involved in pneumatic and hydraulic applications where he supervised product distribution throughout the western United States, Canada, and Mexico. While in this role, he was able to help provide technical and application-specific expertise to customers and distribution to drive specifications.