See how to do it right. Includes video, step by step instructions, and tools list.
Tapered pipe threads are one of the most common end connections found in industry. They are relatively simple to make up, however they always need a sealant since there are designed-in gaps between the male and female threads. This 3-minute clip shows how to apply PTFE tape, a thread sealant used on male tapered pipe threads:
Browse more videos on assembly, installation, identification, product features, and tools.
There are many different sealants available. One of the most popular is PTFE tape. The letters stand for polytetrafluoroethylene. It's a thin film that fills in the gaps between the roots and crests of tapered pipe threads. PTFE tape lubricates the threads, which allows them to be more easily screwed together, to the point of deformation, which is what creates the seal.
Swagelok PTFE tape provides reliable sealing on metal pipe threads in applications up to 450 degrees Fahrenheit, or 230 degrees Celsius. It conforms to Commercial Item Description A-A-58092.
To properly apply PTFE tape, you'll need a couple of tools in addition to the roll of tape:
Make sure that PTFE is right for the job. It should be used only on male tapered pipe threads. Do not use it on straight threads such as those used on flared, coned or tube fitting ends.
Once the connection is tight, do not loosen it. Doing so could mean leakage at the pipe thread. That's all there is to it.
Leaks are common, and small ones are often hard to find. Use our engineers to track down argon, helium, nitrogen, and CDA leaks as small as 1 x10-3 cm3/s. Then get a hand quantifying each leak and choosing cost-effective ways to tighten up.
In our Swagelok Tube Fitting Safety Seminar, our Swagelok certified trainers will show you how to properly apply PTFE thread sealant and other sealants and lubricants, and then ask you to do it yourself under their watchful eye.
You will also learn about pipe fittings, tubing handling, how to correctly install a Swagelok tube fitting, and more.
Here are just three examples of tool and equipment rentals we offer:
More articles like this: