"Innovative design features make maintenance easier."
- From Mechanical seal support systems help reduce costs (Video Below)
Swagelok doesn't make pumps or mechanical seals, but we do have 70 years of expertise in fluid systems themselves. One of the areas where we bring that expertise is mechanical seal support.
Our customers have told us time and again that elimination of leak points is critical for mechanical seal support. Having fewer leak points not only increases the reliability of the system, but it reduces the time needed to audit those connections.
Based on customer feedback, we developed several products to address their specific needs.
When designing these seal support systems, Swagelok kept a number of things in mind. At the top of the list was maintainablity. For example, wherever possible we use U-shaped tubes, allowing components to be removed from the systems without too much trouble.
Another example is using bypass lines on filters. When the filter element needs to be cleaned out or replaced, the flow can be diverted around the filter without stopping the flow through the system.
We also offer customers not just the entire seal support system (such as a seal pot on a stand), but also a connection kit. Seal support kits reduce installation errors and the potential for costly rework. Having the kits and seal support systems available with just a single part number allows for ease of ordering and ease of maintainability within the customer's business systems.
Critical spares such as the fittings — or even entire seal support systems — can be stocked locally. When you need them, you can have them right away.
We have a short video that illustrates the products and designs we've described in this post.
Take a look, then call us at 510-933-6200 or send a note through our website to get the seal support system you need.
More like this: