Share this
What Is a Manifold in the Oil and Gas Industry?
by Morgan Zealear on 11/29/22 9:00 AM
Manifolds assist in the smooth distribution of fluid from a single source to multiple outputs or vice versa. In oil and gas industry applications you might see one used when fluid has to be transferred from wells to test lines or from the storage tank to the production line. Let's look at how manifolds work and how to choose one.
The typical manifold has a hollow structure with arrangements including valves, fittings (tees/ elbow/ plugs), tubes, pipes, and pressure equipment. The hollow body of the manifold allows the fluid to maneuver through the different ports to the production line without any obstruction. The flow parameter is controlled by two-, three-, or five-valve configurations including needle, ball, or bleed valves.
Fighting corrosion
Most manifolds are made out of strong and corrosion-resistant materials to counteract the chemically reactive nature of the process fluids. This is especially true where carbonic acid or hydrogen sulfide is a major corrosive agent.
The role of manifolds in oil and gas
Most manifolds used in the industry are made of stainless steel. Besides the material selection, there are other important considerations for the selection of the right manifold for the oil and gas industry.
- The manifold should be able to handle the maximum allowable working pressure (MAWP) to which it is exposed. The MAWP for oil and gas manifolds can reach as high as 6000 psig.
- The manifold selection should be based on its ability to adjust to extreme temperature limits which can include from the range of -65°F to 1200°F.
- Apart from stainless steel, aluminum, plastic, or iron may be used based on the strength and wear resistance requirement.
- Reduced chances of oil leaks and spills
- Organized flow path which is also easy to maintain
- Smooth and shorter flow path means less fluctuation in fluid temperature and pressure
- The simpler, all-in-one design reduces installation costs
Swagelok’s manifold systems
Whether you are initiating a gas distribution system design or upgrading an existing one, Swagelok offers customized installations of our manifold system to fit your unique specifications. Most Swagelok manifolds feed multiple outlets. Our range of manifold systems includes:
- VB, and VL series (two-, three-, and five-valve) instrument manifolds
- VE series (two-, three-, and five-valve) direct-mount manifolds
- Two-valve remote-mount manifolds
- Mod 85 modular instrumentation systems
The two-valve manifolds are suitable for static pressure and liquid level application while the three- and five-valve manifolds serve application with various pressure differentials. Here are some other features that Swagelok manifolds offer:
- 316 stainless steel construction provides corrosion resistance and required strength
- Smooth internal finish minimizes chances of leaks and promotes smooth flow
- Metal-to-metal sealing with parallelly threaded connection eliminates the requirement for O-ring
- Large or small bonnet needle valve to isolate, equality or bleed off the pressure
- Customizable/ modular manifold construction
- Low fugitive emissions
Installing a Swagelok manifold at your facility
Apart from providing high-quality manifolds, Swagelok can also help you custom fabricate and install them at your Northern California facility. Whether your need is to regulate the flow through multiple cylinders or effectively grab samples for monitoring the process at the sample stations, Swagelok can help with custom-designed installations utilizing our manifolds.
Our manifolds can be customized to fit vertically or horizontally to adjust to any facility space constraints. Our experts can help you understand what a manifold is in the oil and gas industry and also assist in selecting the right tubes, pressure regulators, and connectors. As all the components work in unison with your manifold system, you can be sure about the effective handling of your systems’ process requirements.
About Morgan Zealear| Technical Services Manager
Morgan holds a Bachelor of Science in mechanical engineering from University of California at Santa Barbara. He is certified in Section IX, Grab Sample Panel Configuration and Mechanical Efficiency Program Specification (API 682), and he is well versed in B31.3 Process Piping Code. Before joining Swagelok Northern, he was a manufacturing engineer at Sierra Instruments, primarily focused on capillary thermal meters for the semiconductor industry (ASML).
Related content
Share this
- Archive (465)
- Assembly Services (207)
- About (100)
- Seal Support Systems (96)
- Best Practices (88)
- Training Services (74)
- Fittings (51)
- Semiconductor Applications (49)
- Hoses and Flexible Tubing (47)
- Regulators (44)
- Tubing (42)
- Grab Sampling Systems (32)
- Sampling Systems (32)
- Gas Systems (30)
- Services (30)
- Downloads (29)
- Valves (24)
- Application Support (18)
- Orbital Welding (17)
- Case Studies (13)
- Steam Systems (13)
- Frequently Asked Questions (12)
- Tools (12)
- Measurement Devices (7)
- Subsystems (6)
- Thermal Management (6)
- September 2023 (1)
- August 2023 (2)
- June 2023 (1)
- March 2023 (3)
- February 2023 (3)
- January 2023 (4)
- December 2022 (4)
- November 2022 (4)
- October 2022 (4)
- September 2022 (1)
- August 2022 (3)
- July 2022 (2)
- June 2022 (4)
- May 2022 (1)
- April 2022 (2)
- March 2022 (1)
- February 2022 (2)
- January 2022 (3)
- December 2021 (1)
- November 2021 (6)
- October 2021 (6)
- September 2021 (8)
- August 2021 (4)
- July 2021 (3)
- June 2021 (6)
- May 2021 (6)
- April 2021 (7)
- March 2021 (5)
- February 2021 (4)
- January 2021 (6)
- December 2020 (5)
- November 2020 (6)
- October 2020 (6)
- September 2020 (8)
- August 2020 (7)
- July 2020 (8)
- June 2020 (8)
- May 2020 (6)
- April 2020 (9)
- March 2020 (7)
- February 2020 (10)
- January 2020 (21)
- December 2019 (23)
- November 2019 (21)
- October 2019 (22)
- September 2019 (21)
- August 2019 (22)
- July 2019 (23)
- June 2019 (20)
- May 2019 (23)
- April 2019 (22)
- March 2019 (21)
- February 2019 (20)
- January 2019 (21)
- December 2018 (14)
- November 2018 (19)
- October 2018 (23)
- September 2018 (17)
- August 2018 (29)
- July 2018 (11)
- June 2018 (6)
- May 2018 (5)
- April 2018 (4)
- March 2018 (5)
- February 2018 (3)
- January 2018 (3)
- December 2017 (2)
- November 2017 (4)
- October 2017 (3)
- September 2017 (2)
- August 2017 (6)
- July 2017 (4)
- June 2017 (4)
- May 2017 (4)
- April 2017 (3)
- March 2017 (4)
- February 2017 (3)
- January 2017 (3)
- December 2016 (3)
- November 2016 (3)
- October 2016 (3)
- September 2016 (5)
- August 2016 (5)
- July 2016 (4)
- June 2016 (5)
- May 2016 (3)
- April 2016 (4)
- March 2016 (5)
- February 2016 (11)
- January 2016 (1)
- December 2015 (3)
- November 2015 (4)
- October 2015 (3)
- September 2015 (4)
- August 2015 (4)
- July 2015 (8)
- June 2015 (5)
- May 2015 (3)
- April 2015 (4)
- March 2015 (4)
- February 2015 (3)
- January 2015 (4)
- December 2014 (2)
- November 2014 (3)
- October 2014 (4)
- September 2014 (4)
- August 2014 (4)
- July 2014 (5)
- June 2014 (4)
- May 2014 (4)
- April 2014 (5)
- March 2014 (4)
- February 2014 (3)
- January 2014 (4)
- December 2013 (5)
- November 2013 (3)
- October 2013 (4)
- September 2013 (3)
- August 2013 (5)
- July 2013 (5)
- June 2013 (5)
- May 2013 (3)
- April 2013 (6)
- March 2013 (4)
- February 2013 (4)
- January 2013 (8)
- December 2012 (4)
- November 2012 (6)
- October 2012 (6)
- September 2012 (4)
- August 2012 (4)
- July 2012 (4)
- June 2012 (4)

.webp?width=210&height=70&name=StickyLogo%20(5).webp)